The Full Extension - Disconnect range is designed for the type of application when you need to remove the draw frequently so as to gain either extra access to the draw or to the area behind the draw. This is done by simply pressing the leave on the side of the slide and the 3rd section of the slide will disconnect from the rest of the slide allowing you to remove the draw. All of the slides in this range also come with a self-closing mechanism to avoid any risk of injury or damage to the slide if the draw is removed and the slides are left out. All the slides in this range are also made from Cold Rolled Steel Zinc Plated to allow for extra strength to keep the slide in shape when removing the 3rd tier.
Drawer Slides - Full Extn - Disconnect
Company registration no: 00496138
Company VAT number GB 408154022
Alexia House, Glenmore Business Park
PO19 7BJ Chichester
United Kingdom
0333 207 4497
sales@wixroyd.com