The Simple Draw Latches are usually used for either securing lids to secure box units or latching an item to some sort of work bench or surface. These come in various different designs and styles depending on what the application is that they are required for. For example sprung loaded draw latches to ensure that the box unit lid is securely held on under tension, this would be most commonly used on a roof box for a car or similar application to ensure that the lid stays on even if the car is moving at a high speed.
Draw Latches - Simple