The Range of Torque and Positioning Hinges is a specially designed range with a Torque damper system already built in to the hinge so that you can have a hinge that will work with a smooth motion rather than letting the application slam shut. The Advantage to using one of these over one of the Torque Dampers as that the system is already built into the hinge so you will not need to worry about incorporating the torque damper into your design.
Torque and Positioning Hinges