The push to close paddle latches are defined to sit as smoothly and as flat as possible to the application to keep with the sleek look. These are produced with specially designed cam to allow the slam action closure of the door or panel. These also come with an added safety feature which means that when the key is locked out this prevents movement of the paddle rather than securing the cam so that the cam can still be operated from the inside to prevent a lock in.
pull to open - slam action - standard cylinder lock - steel or stainless
2recessed handle - standard cylinder lock - polyamide
1Push-to-Close Paddle Latches