Wixroyd has a large range of door removal hinges also known as Lift-off hinges these come in 2 grades heavy duty for full size doors or light duty for small scale cabinet doors, there is also a wide range of materials in each grade depending on the application. The majority of these will have a maximum opening angle of 110 degrees, with one exception for the S2402 which will open to a 180 degree if required.
Door Removal Hinges