Our Range of lid stays consists of a number of different stays depending on the function of the lid you require these on. Firstly you will need to identify the way that the lid opens for example either upward opening or top opening. From here you will then note that we have various different stays depending on what you require from them, either to have a positive stop so the lid is held at a fixed point or a Multi-stop stay for stays where the holding point will vary and the lid can be held at multiple angles during the opening motion. Our stays come in either AISI 304 Stainless steel or Zinc plated Steel depending on where the application is that you require them, either external or internal.
Lid Stays